5G NR

Carrier Real-Time Uplink

The features described in this topic apply to the M9484C VXG only.

This topic describes the parameters under the Carrier tab when Capability is set to Real-time Uplink.

UL FRC Config

NTN FRC Config

Export 89600 VSA Setup (Carrier)

Carrier Node Pane

General

Enabled

Spectrum Control

DC Punctured

Baseband Filter

Cell-Specific

Carrier Type

Cell ID

Bandwidth

Numerology Mode

Numerology

Max RB

k0

Configured Bandwidth

Frequency Offset of Point A

Base Sample Rate

Uplink

Channel Allocation and Summary Area

General

Enabled

Applies to the M9484C only.

Displays the component carrier state as either on or off.

GUI Location

Apps > 5G NR > Waveform > Capability set to Real-time Uplink > Carrier > General > Enabled

SCPI Command

[:SOURce]:RADio:NR5G:WAVeform:RTIMe:CCARrier:[STATe]?

SCPI Example

 

Preset

ON

State Saved

Yes

Initial S/W Revision

A.10.00

Spectrum Control

DC Punctured

Applies to the M9484C only.

When DC Punctured is enabled, the DC subcarrier is excluded from the generated signal.

In an orthogonal frequency division multiplexing (OFDM) or orthogonal frequency division multiple access (OFDMA) signal, the subcarrier whose frequency would be equal to the RF center frequency of the station is referred to as the DC subcarrier.

For uplink carrier with Transform Precoding enabled for UL-SCH, DC Punctured is forced to Off.

GUI Location

Apps > 5G NR > Waveform > Capability set to Real-time Uplink > Carrier > Spectrum Control > DC Punctured

SCPI Command

[:SOURce]:RADio:NR5G:WAVeform:RTIMe:CCARrier:DC:PUNCtured[:STATe] ON|OFF|1|0

[:SOURce]:RADio:NR5G:WAVeform:RTIMe:CCARrier:DC:PUNCtured[:STATe]?

SCPI Example

 

Preset

OFF

State Saved

Yes

Initial S/W Revision

A.10.00

Baseband Filter

Applies to the M9484C only.

Enables or disables the baseband filter.

The filter is applied to each numerology of this carrier. It is a low-pass or band-pass FIR filter with hamming window. The central frequency and bandwidth of this filter depend on the resource allocation of each numerology.

Taps: 1024

Band margin: 1 RB for each side

Only available when the carrier type is a downlink or uplink. Not applicable for PRACH.

It is recommended to enable baseband filter to achieve a balance between ACPR and EVM performance.

GUI Location

Apps > 5G NR > Waveform > Capability set to Real-time Uplink > Carrier > Carrier Downlink > Spectrum Control > Baseband Filter

SCPI Command

[:SOURce]:RADio:NR5G:WAVeform:RTIMe:CCARrier:BFILter[:STATe] ON|OFF|1|0

[:SOURce]:RADio:NR5G:WAVeform:RTIMe:CCARrier:BFILter[:STATe]?

SCPI Example

 

Preset

ON

State Saved

Yes

Initial S/W Revision

A.10.00

Cell-Specific

Carrier Type

Applies to the M9484C only.

Displays the component carrier type (Uplink).

GUI Location

Apps > 5G NR > Waveform > Capability set to Real-time Uplink > Carrier > Cell-Specific > Carrier Type

SCPI Command

[:SOURce]:RADio:NR5G:WAVeform:RTIMe:CCARrier:TYPe?

SCPI Example

 

Preset

UL

State Saved

Yes

Initial S/W Revision

A.10.00

Cell ID

Applies to the M9484C only.

Specifies the Cell ID for the component carrier. The Cell ID is used in equations in the physical layer definition to compute synchronization sequences and other values.

GUI Location

Apps > 5G NR > Waveform > Capability set to Real-time Uplink > Carrier > Cell-Specific > Cell ID

SCPI Command

[:SOURce]:RADio:NR5G:WAVeform:RTIMe:CCARrier:CIDentity <integer>

[:SOURce]:RADio:NR5G:WAVeform:RTIMe:CCARrier:CIDentity?

SCPI Example

 

Preset

0

State Saved

Yes

Min

0

Max

1007

Initial S/W Revision

A.10.00

Bandwidth

Applies to the M9484C only.

Sets the component carrier's frequency range and bandwidth.

When bandwidth changes, the MaxRB (for single numerology mode) or N_grid_size(for multiple numerologies mode) is automatically updated based on the table in TS38.101-1 for FR1 and TS38.101-2 for FR2.

GUI Location

Apps > 5G NR > Waveform > Capability set to Real-time Uplink > Carrier > Cell-Specific > Bandwidth

SCPI Command

[:SOURce]:RADio:NR5G:WAVeform:RTIMe:CCARrier:BWIDth FR1BW5M|FR1BW10M|FR1BW15M|FR1BW20M|FR1BW25M|FR1BW30M|FR1BW40M|FR1BW50M|FR1BW60M|FR1BW70M|FR1BW80M|FR1BW90M|FR1BW100M|FR2BW50M|FR2BW100M|FR2BW200M

[:SOURce]:RADio:NR5G:WAVeform:RTIMe:CCARrier:BWIDth?

SCPI Example

 

Couplings

FR2BW200M cannot be supported for Mu2 (60Khz SCS).

Preset

FR1BW100M

State Saved

Yes

Initial S/W Revision

A.10.00

Numerology Mode

Applies to the M9484C only.

Displays the numerology mode of carrier as either single or multiple numerologies.

Only single numerology is supported for an RT Uplink carrier.

GUI Location

Apps > 5G NR > Waveform > Capability set to Real-time Uplink > Carrier > Cell-Specific > Numerology Mode

SCPI Command

[:SOURce]:RADio:NR5G:WAVeform:RTIMe:CCARrier:NUMerology:MODE?

SCPI Example

 

Preset

SINGle

State Saved

Yes

Initial S/W Revision

A.10.00

Numerology

Applies to the M9484C only.

Choices:

MU0 = 0:15 kHz

MU1 = 30 kHz

MU2Ncp = 60 kHz Normal CP

MU3 = 120 kHz

Sets the numerology for the component carrier in single numerology mode. Setting this value reverts the Max RB for valid numerologies to default and resets the user-defined values to those defined in 3GPP specification 38.104 table 5.3.2-1 and 5.3.2-2. This value also determines the set of valid numerology that can be used by a resource allocation within the carrier.

This parameter is only visible in single numerology mode, and it will determine the numerology of all the channels/BWPs in this carrier.

The 15 kHz/30 kHz subcarrier spacing can be used only in frequency range 1 (FR1); 120 kHz/240 kHz subcarrier spacing can be used only in frequency range 2 (FR2); 60 kHz subcarrier spacing can be used in either FR1 or FR2.

Cyclic Prefix (CP) length specifies the symbols per slot. For normal, each slot occupies 14 symbols and for extended each slot occupies 12 symbols. Extended CP is used for subcarrier spacing (SCS) of 60 kHz only. Normal CP length = 7.03125% the length of the symbol and extended CP length = 25% of the length of a signal.

GUI Location

Apps > 5G NR > Waveform > Capability set to Real-time Uplink > Carrier > Cell-Specific > Numerology

SCPI Command

[:SOURce]:RADio:NR5G:WAVeform:RTIMe:CCARrier:SNUMerology MU0|MU1|MU2Ncp|MU3

[:SOURce]:RADio:NR5G:WAVeform:RTIMe:CCARrier:SNUMerology?

SCPI Example

 

Preset

MU1

State Saved

Yes

Initial S/W Revision

A.10.00

Max RB

Applies to the M9484C only.

Sets the maximum number of RB for current numerology of the carrier in Single Numerology mode. The default value is the max RB size for the numerology based on the selected Bandwidth.

This parameter is only visible in Single Numerology mode, it determines the bandwidth of current carrier, the center of carrier is assumed at the middle of whole RB range if k0 is 0, and the N_grid_start for selected numerology is 0.

GUI Location

Apps > 5G NR > Waveform > Capability set to Real-time Uplink > Carrier > Cell-Specific > Max RB

SCPI Command

[:SOURce]:RADio:NR5G:WAVeform:RTIMe:CCARrier:SNUMerology:RB:NUMBer <integer>

[:SOURce]:RADio:NR5G:WAVeform:RTIMe:CCARrier:SNUMerology:RB:NUMBer?

SCPI Example

 

Preset

273

State Saved

Yes

Min

6

Max

275

Initial S/W Revision

A.10.00

k0

Applies to the M9484C only.

Specifies k0 in the single numerology mode to -6, 0, or 6. It is used to adjust the center of the carrier.

GUI Location

Apps > 5G NR > Waveform > Capability set to Real-time Uplink > Carrier > Cell-Specific > k0

SCPI Command

[:SOURce]:RADio:NR5G:WAVeform:RTIMe:CCARrier:SNUMerology:K0MU <real>

[:SOURce]:RADio:NR5G:WAVeform:RTIMe:CCARrier:SNUMerology:K0MU?

SCPI Example

 

Preset

0

State Saved

Yes

Min

-6

Max

6

Initial S/W Revision

A.10.00

Configured Bandwidth

Applies to the M9484C only.

Displays the configured bandwidth of the carrier and is calculated by the maximum bandwidth between each enabled numerology.

GUI Location

Apps > 5G NR > Waveform > Capability set to Real-time Uplink > Carrier > Cell-Specific > Configured Bandwidth

SCPI Command

[:SOURce]:RADio:NR5G:WAVeform:RTIMe:CCARrier:CBWidth?

SCPI Example

 

Preset

98280000

State Saved

Yes

Initial S/W Revision

A.10.00

Frequency Offset of Point A

Applies to the M9484C only.

Displays the relative location (in Hz) of Point A from the middle of the carrier.

GUI Location

Apps > 5G NR > Waveform > Capability set to Real-time Uplink > Carrier > Cell-Specific > Frequency Offset of Point A

SCPI Command

[:SOURce]:RADio:NR5G:WAVeform:RTIMe:CCARrier:APOint:FREQuency:OFFSet?

SCPI Example

 

Preset

-49140000

State Saved

Yes

Initial S/W Revision

A.10.00

Base Sample Rate

Applies to the M9484C only.

Displays the current carrier’s base sample rate, which is calculated automatically.

GUI Location

Apps > 5G NR > Waveform > Capability set to Real-time Uplink > Carrier > Cell-Specific > Base Sample Rate

SCPI Command

[:SOURce]:RADio:NR5G:WAVeform:RTIMe:CCARrier:SRATe?

SCPI Example

 

Preset

122880000

State Saved

Yes

Initial S/W Revision

A.10.00

UL FRC Update for 38.141 v16.9.0

Waveform